Technical FAQs

Ask a Question

What is the part number for a start stop push button kit for the 8536SC NEMA size 1 starters?

Product Line: 
NEMA starters and accessories

Resolution: 
For the NEMA 1 type enclosures use the 9999SA2 kit
for NEMA type 12/3R enclosures use the 9999SA3 kit (user made openings will be needed to field install these kits)
for NEMA 4/4X stainless enclosures use the 9999SA13 kit (user made openings will be needed to field install these kits) 
 
Was this helpful?
What can we do to improve the information ?