Technical FAQs

Ask a Question

What are the part numbers for the auxiliary contacts for the melting alloy NEMA overload relays?

Product Line: 
NEMA Melting Alloy Overload Relays

Resolution: 
For the NEMA size 00-6 type SA-SH there are three parts kits
The replacement normally closed overload contact 9999SO1
The N.O. isolated alarm contact plus N.C. overload contact 9999SO4
and the N.C. isolated alarm contact plus N.C. overload contact 9999SO5
Was this helpful?
What can we do to improve the information ?