Technical FAQs

Ask a Question

Can the firmware be upgraded in the Micrologic trip units of Powerpact H, J and L circuit breakers?

Product Line;
Circuit Breakers

Environment;
Powerpact H, J and L, with Micrologic trip units

Resolution;
All of the information is in the trip units is hard-coded into the hardware, and cannot be upgraded.
 
Was this helpful?
What can we do to improve the information ?