Technical FAQs

Ask a Question

Video: Can the 2510F be mounted into a single gang junction box for retrofit?

Issue:
Can the 2510F be mounted into a single gang junction box for retrofit?

Product Line:
2510F NEMA Starters - GIC Product

Environment:
US Product

Cause:
Product Installation

Resolution:
Yes, the 2510F Fractional Horsepower manual motor starter comes in a variety of enclosures including Nema 1, Nema 4, and Nema 3R/7/9 as well as an option for a flush plate. Open types without a pilot light fit standard single gang switch boxes, and can be used with any cover plate having a standard toggle cutout. Single-unit flush mounting types, including those with pilot light, are suitable for wall mounting in a standard switch box or for machine cavity mounting without a box.  Please see attached video showing the Stainless steel flush plate offering and mounting.

 
Was this helpful?
What can we do to improve the information ?