Technical FAQs

Ask a Question

Video: How to use the limited torque "throw-away" screws for the Powerpact B-frame breaker

Issue:
How to use the limited torque "throw-away" screws for the Powerpact B-frame breaker
 
Product Line:
Powerpact Molded Case Circuit Breakers
 
Environment:
B-frame Circuit Breakers
 
Resolution:
You would place the screw onto the lug on the breaker, and use an allen wrench to tighten it until the green (80 in-lbs) or yellow (44 in-lbs) cover breaks. For further instruction, see the video below:

Was this helpful?
What can we do to improve the information ?