Technical FAQs

Ask a Question

Can the ventilated section of a NC VS or NC VF be removed and used on a NC S or NC F cover?

Issue: 
Can the ventilated section of a NC VS or NC VF be removed and used on a NC S or NC F cover?

Product Line: 
Panelboards

Environment: 
NF, NQ, cover, Mono-Flat Front, vented cover

Cause:
Ordered a non vented cover in error.  

Resolution:
No. The vents are welded as part of the trim and are not removable.  
 
Was this helpful?
What can we do to improve the information ?