Technical FAQs

Ask a Question

What does warning 8000 mean on a GT250?

Issue:
Warning code 8000 appeared on the display.

Product Line:
GT250

Environment:

Cause:
This is a result of a dual power supply upgrade

Resolution:
A dual power supply upgrade creates a redundancy in the GT250 model. If one of the power supplies go down, the unit will continue to function with only one power supply. The warning 8000 will notify the customer that a power supply needs to be replaced.
Was this helpful?
What can we do to improve the information ?