Technical FAQs

Ask a Question

Do the all of the 9070 control power transformers have the same mounting hole patterns and dimensions?

Issue:
Do the all of the 9070 control power transformers have the same mounting hole patterns and dimensions?

Product Line:
Control Power Transformers

Environment:
9070 type T and 9070 type TF transformers.

Cause:
Dimensional information

Resolution:
No, the bases are different within the various sizes of the control power transformers. Please reference the 9070CT9901 control power transformer catalog.

http://www2.schneider-electric.com/resources/sites/SCHNEIDER_ELECTRIC/content/live/FAQS/268000/FA268443/en_US/9070CT9901.pdf



 
Was this helpful?
What can we do to improve the information ?