Technical FAQs

Ask a Question

How long is the handle on a 9421LJ4?

Issue:
How long is the handle on a 9421LJ4?

Product Line: 
Nema OP & Door Mechanisms 

Environment: 
Contactors, Starters OP 

Cause: 
Dimensions

Resolution: 
 6 inches is the length -  this can be found on page 8-21, digest 177

 
Was this helpful?
What can we do to improve the information ?