Technical FAQs

Ask a Question

Do the ATV630 come with Conduit Entrance Kits installed?

Issue:
 Do the ATV630 come with Conduit Entrance Kits installed?

Product Line:
All ATV630 drives
 
Environment:
Conduit Entrance Kits
 
Cause:
n/a
 
Resolution:
For the ATV630 Frame Size 1-4 the Conduit Entrance kits come already Installed on the drive.
For Frame Size 5, they are supplied, but they are not installed on the drive.
For Frame Size 6, they are not supplied and have to be ordered .  The part number is VW3A9704.


 
Was this helpful?
What can we do to improve the information ?