Technical FAQs

Ask a Question

Are buck boost transformers available in stainless steel enclosures?

Issue:
Are buck boost transformers available in stainless steel enclosures?

Product Line:
Transformers

Environment:
Buck Boost Enclosures

Cause:
Stainless Steel options 

Resolution:
Yes, but only as a special quote from the plant.  The Distributor will need to request a quote from the account Rep or Field office to get a quote.


 
Was this helpful?
What can we do to improve the information ?