Technical FAQs

Ask a Question

What are the dimensions of the HOMC21UC load center cover?

Issue:
Product Design features

Product Line:
Homeline Load Centers

Environment:
Dimensions

Cause:
Installation

Resolution:

This cover is approximately 22.12" H x 15.44" W. The cover will overlap the load center enclosure by approximately 0.60" (19/32``) on all sides.
Was this helpful?
What can we do to improve the information ?