Technical FAQs

Ask a Question

ATV212: Why is my drive not resetting the current fault?

Issue:  
ATV21/ATV212 is not resetting the current fault even if you cycle power

Product Line: 
All ATV21/212 drives

Environment: 
Resetting the fault

Cause:
n/a

Resolution:  
Ensure that F602 (Drive Fault Memory), is set to 0 - the fault memory is cleared.
 
Was this helpful?
What can we do to improve the information ?