Technical FAQs

Ask a Question

What main breakers are used in the EZM3800GCBE and EZM3800JCBE Series M01 Main Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Main Breaker

Cause:
Application

Resolution:
The main breaker used are as shown below and these breakers are Not adjustable.
1) The EZM3800GCBE uses the MGF36800
2) The EZM3800JCBE uses the MJF36800
Was this helpful?
What can we do to improve the information ?