Technical FAQs

Ask a Question

Where can I find the Installation Instructions for a TVS2EMA32A external mounted TVSS?

Issue:
Where can I  find the Installation Instructions for a TVS2EMA32A external mounted TVSS?

Product Line:
TVSS, Surge Protection Devices,  SPD

Environment:
Installation Bulletin for EMA Surge Protection Devises used in the United States

Cause: 
Customer needs to know how to Install SPD externally.

Resolution:
Please refer to the Instruction Bulletin for the EMA Surge Protectors.  
For additional One-On-One assistance please contact us direct at 800-577-7353 or 888-778-2733 option 1.  
Was this helpful?
What can we do to improve the information ?