Technical FAQs

Ask a Question

What is the part number for the top, side, rear and front cover, core leg and base assembly for the EX75T3H (20K enclosure) transformer?

Issue:
What is the part number for the top, side, rear and front cover, core leg and base assembly for the EX75T3H (20K enclosure) transformer?

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Ventilated EX Transformers by SquareD/Schneider Electric

Cause:
Customer needs replacement covers which were damaged. 

Resolution:
The replacement covers for a 20K enclosure for the EX75T3H transformer. 
Top Cover: EAV85836
Side panel: EVA85835
Front Cover with labels:  EVA85837
Rear Cover:  EAV85838 
Rear Shield:  NHA14634  
Base Core Leg:  EAV94531 
Base Assembly:  EAV85833 
Was this helpful?
What can we do to improve the information ?