Technical FAQs

Ask a Question

Instruction Bulletin and programming the Reactivar AV5000 and AV6000 Powerfactor Correction Capacitors - PFC.

Issue:
Instruction Bulletin and programming the Reactivar AV5000 and AV6000 Powerfactor Correction Capacitors - PFC.

Product Line:
Powerfactor Correction Capacitors - PFC

Environment:
Reactivar AV5000 and AV6000

Cause:
Programming assistance required

Resolution:
Refer to page 27 in the 5830IB0901 instruction manual for the AV5000/AV6000 capacitors. Parameter values will need to be calculated from the data provided at the time of order. Refer to the drawings or the BOM provided at the time of order. See the attachment below for the instruction manual.
Was this helpful?
What can we do to improve the information ?