Technical FAQs

Ask a Question

Solid State Overload Relays with High Efficiency Motors

Issue:
Can the 9065 Solid State Overloads be used with high efficiency motors

Product Line:
9065 Solid State Overload Relays - GIC Product

Environment:
US Product

Cause:
Product Application

Resolution:
In general, the solid state overload relays can be used with high efficiency motors.  The manufacturer of the motor should first be consulted though as the initial inrush can sometimes be sufficient to nuisance trip the relay on start up.  Compare the inrush of the motor to the trip curves specified by the instruction bulletin for the relay to make an absolute determination.
Was this helpful?
What can we do to improve the information ?