Technical FAQs

Ask a Question

Where can I find the dimensions for the CF2308GLFM11 elbow?

Issue:
Where can I find the dimensions for the CF2308GLFM11 elbow?

Product Line:
I-Line II Busway, 800A - 5000A Busway 

Environment:
USA Busway, Flatters Elbow, Fittings (All Feeder Style) 

Cause:
Customer needs the dimensions. 

Resolution:
Dimensions for the CF2308GLFM11 elbow can be found in the  Busway Systems Catalog, 5600CT9101R09/12, page 74. 
See Attached
Was this helpful?
What can we do to improve the information ?