Technical FAQs

Ask a Question

ATV630 - How do I set the reference template to Pedestal?

Issue:
ATV630 - How do I set the reference template to Pedestal?

Product Line:
ATV600 series drives

Environment:
All models, All serial numbers

Cause:
Information unavailable or difficult to locate in current literature.

Resolution:
The Reference Template parameter can be found by navigating from the main menu into COMPLETE SETTINGS, then GENERIC FUNCTIONS, SPEED LIMITS, REFERENCE TEMPLATE.
 
Was this helpful?
What can we do to improve the information ?