Technical FAQs

Ask a Question

How many XVU illuminated lens can be stacked together

Product line:
XVU Tower Lights:

Resolution: 
XVU tower lights are customer assembled signaling units that are mounted on the body of the unit with a mounting accessory.
• Maximum of 5 illuminated units or 4 illuminated units with 1 audible unit can be
assembled. The illuminated or audible unit stack vertically.
Was this helpful?
What can we do to improve the information ?