Technical FAQs

Ask a Question

What is the power loss for a 9070T200D19 transformer?

Issue: 
What is the power loss for a 9070T200D19 transformer?

Product Line:
industrial Control Transformer, Type T

Environment:
208/240/277/380/480 Vac Primary, 24 Vac Secondary, 200VA 

Cause:
Customer need the BTU's. 

Resolution:
The power loss / heat loss for the 9070T200D19 transformer would be as follows:
100% load = 109 BTU/hr
75% = 82 BTU/hr
50% = 63 BTU/hr
25% = 52 BTU/hr
No Load = 48 BTU/hr
or 31.9 FL total watts
Was this helpful?
What can we do to improve the information ?