Technical FAQs

Ask a Question

What is the Terminal Lug Data for the EZM3600GCBE/JCBE and the EZM3800GCBE/JCBE Main Devices?

Standard Terminal Lug Data

Product Line:
EZM Metering

EZM Main Breaker lugs


The EZM3600GCBE, EZM3600JCBE, EZM3800GCBE and EZM3800JCBE are all designed to meet the West Coast 'EUSERC' Utilities requirementes and do not come standard with lugs from the factory, but contain Lug Landing Pads to meet the EUSERC requirements. Each Lug Landing pad on ALL of these catalog numbers will ONLY accommodate (2) lugs per pad (or 2 lugs per phase/neutral). Which means these EZM main devices will ONLY accommodate (2) wires Per Phase/Neutral. See the below attached CAD drawing showing the part numbers of the lugs and the maximum wire size the lugs will accept. 

Was this helpful?
What can we do to improve the information ?