Technical FAQs

Ask a Question

Proper way to connect (2) ATV320 for Bus Sharing

Issue:
ATV320, Altivar 320, Is the proper way to connect (2) ATV320 to one resistor?

Connect ATV320-1 (PA/+) to ATV320-2 (PA/+)
Connect ATV320-1 (PC/-) to ATV320-2 (PC/-)

ATV320-1 (PB) to DB resistor
ATV320-1 (PBe) to DB resistor

Product Line:
ATV320C

Environment:
DC Bus

Cause:
Bus sharing

Resolution:
Response from France:

The  ATV32 and ATV320B, in DC bus sharing point of view are similar  (fuse, fast on connection cable).
For ATV320C it is little different. On ATV320C, there is only terminal, so you don't need  the fast on connection (VW3M2207 ).
For DC bus and braking resistor (there is no PBe) :
Connect ATV320-1 (PA/+) to ATV320-2 (PA/+)
Connect ATV320-1 (PC/-) to ATV320-2 (PC/-)
 ATV320-1 (PB) to Braking resistor
Delete this- ATV320-1 (PBe) to braking resistor    
Replace with-  ATV320-1 (PO) to braking resistor
Was this helpful?
What can we do to improve the information ?