Technical FAQs

Ask a Question

Where can I locate the drawing for a 8998SBA040CFTMA

Issue:
Where can I locate the drawing for a 8998SBA040CFTMA, MCC bucket? 

Product Line:
Combination Starter Unit, Class 8998

Environment:
FVNR Combination Starter Units with Motor Circuit Protector Disconnects, HOA Red On / Green Off Lights, NEMA size 3, 40Hp, 18" space

Cause:
Customer requested drawing.

Resolution:
Please refer to the attachment for the 8998SBA040CFTMA drawings.
Was this helpful?
What can we do to improve the information ?