Technical FAQs

Ask a Question

IEC Bimetallic Overload for Open Delta

Which type of IEC Bimetallic overload relay should be used on a high-leg delta system?

Product Line:
LRD Overloads - GIC Product

US Product

Product Selection

Bimetallic LRD units without single phase sensitivity should be used for open delta (high-leg delta) systems.  Standard single phase sensitive LRD units can nuisance trip in these systems due to imbalance.  It is important to note the LRD units without single phase sensitivity will also not have phase loss protection.  An appropriate separate phase loss relay should be selected to provide this type of protection.
Was this helpful?
What can we do to improve the information ?