Technical FAQs

Ask a Question

Do we offer the EX type K13 non-ventilated transformers?

Issue:
Do we offer the EX type K13  non-ventilated transformers?
Product Line:
Transformers

Environment:
EX Three Phase General Purpose Dry Type 600 Volts and Below

Cause:
Customer asking for a K13 rating that is non-ventilated.

Resolution:
No, we do not offer K13 non-ventilated transformers.  The issue is the heat factor requirement for the K13 rating.
Was this helpful?
What can we do to improve the information ?