Technical FAQs

Ask a Question

What is the factory set or default password for the LIM (IG6M or IG6) that are installed in the medical panels?

Issue:
What is the factory set or default password for the LIM (IG6M or IG6) that are installed in the medical panels?

Product Line:
LIM

Environment:
IG6 LIM ( line isolation monitor )

Cause:
Password required

Resolution:
The default password is 807. This is located on page 26 in the instruction bulletin for the IG6M or IG6. These items are also installed in the current style SIP See attachment.
Was this helpful?
What can we do to improve the information ?