Technical FAQs

Ask a Question

How can I enable Dual Generator Support in my Conext ComBox?

Issue:
How can I enable Dual Generator Support in my Conext ComBox?

Product Line:
Conext Series inverter/chargers and accessories

Environment:
Conext ComBox web user interface

Cause:
This feature is not currently discussed in the Owner's Guide for the Conext ComBox

Resolution:
Simply connect AC1 to GEN1, and AC2 to GEN2. Then change the appropriate associations for the inverters and AGS using the ComBox. For example, AC1 Association (Grid) could be set to Generator 1, and AC2 Association (Generator) could be set to Generator 2, or vice versa. Be sure to change these associations, and as an extra precaution, leave SelltoGrid disabled to be sure your generator is protected. Make sure that these associations are also consistent across devices.
Was this helpful?
What can we do to improve the information ?