Technical FAQs

Ask a Question

What are the repair parts for an EZM3600GCBU, Series M01 main circuit breaker unit?

Current design repair parts

Product Line:
EZ Metering Equipment

Repair parts


Only the parts listed below are considered field replaceable:

Top Cover - EZM3600GCBUTC (Includes handle and all labels) 
Bottom Cover  - 7329386372 (includes handle)
Cover Screws - 4020513002K (This is a bag of 10 cover screws)
Main Circuit Breaker - MGP36600
Standard Lugs for Main Circuit Breaker  - AL800M23K (Kit includes 3 Lugs)
Main Neutral Lugs - MMLK500 (Kit inlcudes 3 lugs and the main neutral will accept 2 lugs)
Bonding Strap kit - 7329696750 
Mounting Channel - 7329654302
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP 
Top cover sealing screw - X1299
Removable Bottom Endwall - 7329386551
Bottom endwall mounting screws - 2142717120 (requires 4)

Was this helpful?
What can we do to improve the information ?