Technical FAQs

Ask a Question

What are is the part number for the circuit breaker operating mechanism for the MFLEX?

Issue: 
What are is the part number for the circuit breaker operating mechanism for the MFLEX?
 
Product Line:
MFLEX enclosed  units
 
Environment:
All part number
 
Cause:
Replacement parts
 
Resolution:
 See below:               
Helpful Links          
           
The drive MAY be repairable even if parts are no longer available for sale.  Contact Schneider Electric Industrial Repair Service (SEIRS) at 800-950-9550  
Contact your local Schneider Electric distributor for a replacement drive. (search here)  
New!  Try our Drive and SoftStart selection tool for self selection (open style devices)
Technical Support for AC drives and soft starters: 888-SQUARED (888-778-2733) select option 1 for Technical Support and then option 4 for AC Drives and Softstarts.          
Technical Support is available from 8am EST to 8pm EST M-F and 24 hours a day for EMERGENCIES. 
Was this helpful?
What can we do to improve the information ?