Technical FAQs

Ask a Question

What is LPVT?

LPVT is the acronym for Low Power Voltage Transformer. LPVTs are sensor style VTs (resistive or capacitive dividers) as opposed to traditional iron core transformer style VTs. The output a secondary voltage between 0.2 and 4V and can be used in conjunction with an up converter box to give a 120V output to protective relays and meters.
Was this helpful?
What can we do to improve the information ?