Technical FAQs

Ask a Question

9007C62B2Y19016: What is the Y19016 suffix? 

Issue: 
What is the suffix Y19016 on the 9007C62B2Y19016 limit switch?

Product Line:
9007C Limit Switches, Heavy Duty Industrial Single- and Two-Pole

Environment:
Standard Box Plug-In, 2 NO and 2 NC contacts, Rotary Lever Arm, Pre-travel Spring return, CW & CCW

Cause: 
Determine if the Y19016 is a 5 pin as provided in the On-Line data sheet or a 9 pin. 

Resolution:
The 9007C62B2Y19016 has a pre-wired Brad Harrison 9 pin MINI change connector installed for Chrysler.
Was this helpful?
What can we do to improve the information ?