Technical FAQs

Ask a Question

What is LPVT?



Issue:
What is LPVT?

Product Line:
MV Switchgear components

Environment:
Premset Switchgear components

Cause:
Definition

Resolution:
LPVT is the acronym for Low Power Voltage Transformer. LPVTs are sensor style VTs (resistive or capacitive dividers) as opposed to traditional iron core transformer style VTs. The output a secondary voltage between 0.2 and 4V and can be used in conjunction with an up converter box to give a 120V output to protective relays and meters.
Was this helpful?
What can we do to improve the information ?