Technical FAQs

Ask a Question

Is 2SIS switchgear available in two-high construction?

Issue:
Is 2SIS switchgear available in two-high construction?

Product Line:
MV Switchgear

Environment:
Premset Switchgear

Cause:
Product features and application

Resolution:
No, it is only available in one-high construction.
Was this helpful?
What can we do to improve the information ?