Technical FAQs

Ask a Question

Can I use my Conext Insight to control my system remotely?

Issue:
Customer wants to use Conext Insight for system controls, such as enabling and disabling system settings

Product Line:
Conext Series solar equipment and accessories
 
Environment:
Conext Series solar systems with a Conext ComBox connected
 
Resolution:
Conext Insight is read only. System controls are not available.

Cause:
Conext Insight is a cloud-based system and only receives data from the Conext Combox with an active internet connection.
Was this helpful?
What can we do to improve the information ?