Technical FAQs

Ask a Question

Conext XW+ - unit is powering up in stand by

Issue:
 
A commissioned Conext XW+ powers up in stand by after being powered down
 
Environment:
 
Conext XW+ inverter (6848 / 5548) Legacy XW inverters (6048 / 4548 / 4024)

Resolution:

Units have a battery to save system setting, typically unit should save the settings but if the unit is interrupted during opertion and shut down suddenly, there is a chance when the unit repowers up it could power up in stand by.

To avoid this unit should be put in stand by before the unit is powered down.


NOTE:If the unit has a faulty battery - unit will always power up in stand by - battery is NOT replaceable
 
 
Was this helpful?
What can we do to improve the information ?