Technical FAQs

Ask a Question

What type main breakers are used when converting a QO convertible main load center from main lug to main breaker?

Issue:
Product Feature

Product Line:
QO and HOM LC

Cause:
Clarification

Resolution:
The 125A, 1 phase maximum convertible main lugs load centers would use a QOM1-VH main breaker for this application. The main breaker cannot exceed the ampere rating of the load center.
The 150A, 200A or 225A, 1 phase maximum convertible main lugs load centers would use a QOM2-VH main breaker for this application. The main breaker cannot exceed the ampere rating of the load center.
Three phase main lug load centers are not convertible to main breaker. 
 
Was this helpful?
What can we do to improve the information ?