Technical FAQs

Ask a Question

What main breakers are used in the EZM11000GCBT- GCBU - JCBT- JCBU - GCBE and JCBE Series M01 Main Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Main Breaker

Cause:
Application

Resolution:
The main breaker used are as shown below and these breakers are Not adjustable.
1) The EZM11000GCBT uses the PGM36100U31A
2) The EZM11000GCBU uses the PGP36100U31A
3) The EZM11000JCBT uses the PJM36100U31A
4) The EZM11000JCBU uses the PJP36100U31A
5) The EZM11000GCBE uses the PGF36100U31A
6) The EZM11000JCBE uses the PJF36100U31A
Was this helpful?
What can we do to improve the information ?