Technical FAQs

Ask a Question

What molded case switches are used in the EZM1800FSB - FST and FSE EZM Main Fusible Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Molded Case Switches 

Cause:
Application

Resolution:
The main molded case switches used are as shown below:
1) The EZM1800FSB uses the MJP22000Z80
2) The EZM1800FST uses the MJM22000Z80
3) The EZM1800FSE uses the MJF22000Z80
Was this helpful?
What can we do to improve the information ?