Technical FAQs

Ask a Question

What main breakers are used in the EZM1800GCBT- GCBU - JCBT- JCBU - GCBE and JCBE Series M01 Main Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Main Breaker

Cause:
Application

Resolution:
The main breaker used are as shown below and these breakers are Not adjustable.
1) The EZM1800GCBT uses the MGM26800
2) The EZM1800GCBU uses the MGP26800
3) The EZM1800JCBT uses the MJM26800
4) The EZM1800JCBU uses the MJP26800
5) The EZM1800GCBE uses the MGF26800
6) The EZM1800JCBE uses the MJF26800I
Was this helpful?
What can we do to improve the information ?