Technical FAQs

Ask a Question

What is the part number for the power cable for XUYAFVCO946S

Issue; 
What is the part number for the power cable for XUYAFVCO946S

Product Line;
Sensor

Environment; 
Amplifer for glass fiber sensor

Cause;
power cable

Resolution;
The power cables are:
 
Description Details Length of Cable Catalog Number
 
Pre-wire M8 Connector
 
Straight 2 XZCP0941L2
Pre-wire M8 Connector
 
Elbowed (90) 2 XZCP1041L2
Pre-wire M8 Connector
 
Straight 5 XZCP0941L5
Pre-wire M8 Connector
 
Elbowed (90) 5 XZCP1041L5

 
Was this helpful?
What can we do to improve the information ?