Technical FAQs

Ask a Question

What molded case switches are used in the EZM3600FSB - FST and FSE EZM Main Fusible Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Molded case switches

Cause:
Application

Resolution:
The molded case switches used are as shown below.
1) The EZM3600FSB uses the MJP32000Z60
2) The EZM3600FST uses the MJM32000Z60
3) The EZM3600FSE uses the MJF32000Z60
Was this helpful?
What can we do to improve the information ?