Technical FAQs

Ask a Question

What main breakers are used in the EZM3600GCBT- GCBU - JCBT- JCBU - GCBE and JCBE Series M01 Main Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Main Breaker

Cause:
Application

Resolution:
The main breaker used are as shown below and these breakers are Not adjustable.
1) The EZM3600GCBT uses the MGM36600
2) The EZM3600GCBU uses the MGP36600
3) The EZM3600JCBT uses the MJM36600
4) The EZM3600JCBU uses the MJP36600
5) The EZM3600GCBE uses the MGF36600
6) The EZM3600JCBE uses the MJF36600
Was this helpful?
What can we do to improve the information ?