Technical FAQs

Ask a Question

What molded case switches are used in the EZM1600FSB - FST and FSE EZM Main Fusible Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Molded Case Switches 

Cause:
Application

Resolution:
The main molded case switches used are as shown below:
1) The EZM1600FSB uses the MJP22000Z60
2) The EZM1600FST uses the MJM22000Z60
3) The EZM1600FSE uses the MJF22000Z60
Was this helpful?
What can we do to improve the information ?