Technical FAQs

Ask a Question

What main breakers are used in the EZM1600GCBT- GCBU - JCBT- JCBU - GCBE and JCBE Series M01 Main Devices?

Issue:
Product Design Features

Product Line:
EZM Metering Mains

Environment:
Main Breaker

Cause:
Application

Resolution:
The main breaker used are as shown below and these breakers are Not adjustable.
1) The EZM1600GCBT uses the MGM26600
2) The EZM1600GCBU uses the MGP26600
3) The EZM1600JCBT uses the MJM26600
4) The EZM1600JCBU uses the MJP26600
5) The EZM1600GCBE uses the MGF26600
6) The EZM1600JCBE uses the MJF26600
Was this helpful?
What can we do to improve the information ?