Technical FAQs

Ask a Question

What is included in the QMB400T6 or QMB600T6?

Issue:
What is the QMB400T6 and QMB600T6? 

Product Line:
QMB Switch

Environment:
Applies to the QMB400T6 and QMB600T6.

Cause:
Need to know with how many poles this kit will work?

Resolution:
The QMB400T6 and QMB600T6 is a Class T fuse kit that converts the QMB switch for use with 600V Class T fuses. It can be used in certain 400A (QMB400T6) and 600A (QMB600T6), Series E QMB switches.
Both kits include 6 connector assemblies, two per pole, for a 3 pole switch.  
 
Was this helpful?
What can we do to improve the information ?