Technical FAQs

Ask a Question

Can you provide with the harmonic spectrum up to 60th level for the ATV32 drives?

Issue:
Can you provide with the harmonic spectrum up to 60th level for the ATV32 drives?

Product Line:
ATV32 drives

Environment:
All ATV32 drives

Cause:
Harmonics

Resolution:
Unfortunately, the table is only up to 53th harmonic with and without line choke, the harmonic barely exist over 53th.

 
Was this helpful?
What can we do to improve the information ?