Technical FAQs

Ask a Question

Is there a blank to use on SD75430?

Issue: 
Is there a blank that can be use on SD75430?

Product Line: 
PTLVB-Busways Power IEC & NEMA 

Environment: 
Busway, SD, Plug in Units 

Cause: 
 I Line Plug-in Units  


Resolution: 
There are no spare parts for this Old Busway, sugggest fabricating a blank from a local fabricator. 





 
Was this helpful?
What can we do to improve the information ?