Technical FAQs

Ask a Question

Are Square D safety switches rated for a 25 Hz, DC voltage application?

Issue:
Are Square D safety switches rated for a 25 Hz, DC voltage application?

Product Line:
Fusible and non-fusible safety switches sold and supported in the USA.

Environment:
Application

Cause;
Specifications

Resolution:
The switch itself is fine for 25 Hz, either fusible or non-fusible. However, the customer will have to verify the fuses will work on this application. 
Was this helpful?
What can we do to improve the information ?